FB#.IDENTIFIED
Description
This parameter reports the device type that the drive has successfully identified. Its value is based on FB#.SELECT.
|
Type |
Description |
|---|
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 | |
| Feature Change | 02-06-03-000 | Added support for SSI feedback. |
| Feature Change | 02-12-01-000 | Added BiSS-B Digital types (35, 135). |
General Information
|
Type |
Read Only |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
See Also |
|
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
FB1.IDENTIFIED |
3500h |
23h |
Unsigned8 |
- |
- |
Read only |
No |
|
FB2.IDENTIFIED |
3501h |
23h |
Unsigned8 |
- |
- |
Read only |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
30000 |
1 |
30000 (0x7530) |
FB1.IDENTIFIED |
Signed16 |
Read Only |
Yes |
|
30001 |
1 |
30001 (0x7531) |
FB2.IDENTIFIED |
Signed16 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
FB1.IDENTIFIED |
30000 |
Signed16 |
Read Only |
- |
|
FB2.IDENTIFIED |
30001 |
Signed16 |
Read Only |
- |